Property (Read-Write)
SCPI.FORMat.DATA = Value
Value = SCPI.FORMat.DATA
This command sets/gets a data transfer mode applied for all SCPI connections, applied for all array commands/queries.
|
Parameter |
Value |
|
Description |
Data transfer mode |
|
Data Type |
Character string type (String) |
|
Range |
ASCii: Set data transfer mode to 'ASCii' REAL32:Set data transfer mode to 'IEEE 32 floating point binay' REAL64:Set data transfer mode to 'IEEE 64 floating point binay' |
|
Preset Value |
ASCii |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "ASCii"
SCPI.FORMat.DATA = Var
Var = SCPI.FORMat.DATA
No equivalent key is available on the front panel.
:FORMat:DATA {ASCii|REAL32|REAL64}
:FORMat:DATA?
{ASCii|REAL32|REAL64} <newline><^END>
10 OUTPUT 717;":FORMat:DATA ASCii"
20 OUTPUT 717;":FORMat:DATA ?"
30 ENTER 717;A$