SCPI.INITiate.TR(Ch).IMMediate

Object Type

Method (Write Only)

Syntax

SCPI.INITiate.TR(Ch).IMMediate

Description

This command sets the property to move once to waiting-for-trigger state, for the selected channel Ch.

Examples

SCPI.INITiate.TR1.IMMediate

Related Objects

SCPI.INITiate.TR(Ch).CONTinuous

Equivalent Key

No equivalent key is available on the front panel.

Equivalent SCPI Command

Syntax

:INITiate:TR[1-1]:IMMediate

Example of use

10 OUTPUT 717;":INITiate:TR1:IMMediate"