Property (Read-Write)
SCPI.PROGram.COM.EVENt = Value
Value = SCPI.PROGram.COM.EVENt
This command sets/gets VBA callback.
|
Parameter |
Value |
|
Description |
VBA callback |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
No |
|
Save-Recall Effect |
No |
|
Error |
- |
Dim Var as Boolean
Var= 1
SCPI.PROGram.COM.EVENt = Var
Var = SCPI.PROGram.COM.EVENt
PN Menu: Macro Setup > E5052 Event
SP Menu: Macro Setup > E5052 Event
FP Menu: Macro Setup > E5052 Event
TR Menu: Macro Setup > E5052 Event
AM Menu: Macro Setup > E5052 Event
BB Menu: Macro Setup > E5052 Event
PS Menu: Macro Setup > E5052 Event
USER Menu: Macro Setup > E5052 Event
:PROGram:COM:EVENt {ON|OFF|1|0}
:PROGram:COM:EVENt?
{ON|OFF|1|0} <newline><^END>
10 OUTPUT 717;":PROGram:COM:EVENt 1"
20 OUTPUT 717;":PROGram:COM:EVENt ?"
30 ENTER 717;A