SCPI.PROGram.SKEY.ITEM(1-8).IMMediate

Object Type

Method (Write Only)

Syntax

SCPI.PROGram.SKEY.ITEM(1-8).IMMediate

Description

This command executes user defined key. This command generates an error if either the program is not running, event is not enabled or if the item is not enabled.

Examples

SCPI.PROGram.SKEY.ITEM8.IMMediate

Related Objects

SCPI.PROGram.SKEY.ITEM(1-8).ENABle

SCPI.PROGram.SKEY.ITEM(1-8).LABel

Equivalent Key

PN Menu: Macro Setup > User Menu > User Label 1

SP Menu: Macro Setup > User Menu > User Label 1

FP Menu: Macro Setup > User Menu > User Label 1

TR Menu: Macro Setup > User Menu > User Label 1

AM Menu: Macro Setup > User Menu > User Label 1

BB Menu: Macro Setup > User Menu > User Label 1

USER Menu: Macro Setup > User Menu > User Label 1

Equivalent SCPI Command

Syntax

:PROGram:SKEY:ITEM[1-8]:IMMediate

Example of use

10 OUTPUT 717;":PROGram:SKEY:ITEM8:IMMediate"