Property (Read-Write)
SCPI.SENSe.AM(Ch).FAST = Value
Value = SCPI.SENSe.AM(Ch).FAST
This command sets/gets fast measurement mode, for the selected channel Ch.
|
Parameter |
Value |
|
Description |
Fast measurement mode |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as Boolean
Var= 1
SCPI.SENSe.AM1.FAST = Var
Var = SCPI.SENSe.AM1.FAST
AM Menu: Setup > Fast Measurement
:SENSe:AM[1-1]:FAST {ON|OFF|1|0}
:SENSe:AM[1-1]:FAST?
{ON|OFF|1|0} <newline><^END>
10 OUTPUT 717;":SENSe:AM1:FAST 1"
20 OUTPUT 717;":SENSe:AM1:FAST ?"
30 ENTER 717;A