Property (Read-Write)
SCPI.SENSe.BB(Ch).IFGain = Value
Value = SCPI.SENSe.BB(Ch).IFGain
This command sets/gets IF IFGain 10dB Step, for the selected channel Ch.
|
Parameter |
Value |
|
Description |
IF IFGain 10dB Step |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
0 ~ 50 |
|
Preset Value |
20 |
|
Unit |
dB |
|
Resolution |
10 |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as Double
Var= 0
SCPI.SENSe.BB1.IFGain = Var
Var = SCPI.SENSe.BB1.IFGain
BB Menu: Setup > IF Gain
:SENSe:BB[1-1]:IFGain {0 ~ 50}
:SENSe:BB[1-1]:IFGain?
{0 ~ 50} <newline><^END>
10 OUTPUT 717;":SENSe:BB1:IFGain 0"
20 OUTPUT 717;":SENSe:BB1:IFGain ?"
30 ENTER 717;A