Property (Read-Write)
SCPI.SENSe.DCONverter.INPut = Value
Value = SCPI.SENSe.DCONverter.INPut
This command sets/gets RF Input port.
|
Parameter |
Value |
|
Description |
RF Input port |
|
Data Type |
Character string type (String) |
|
Range |
DCONverter|DIRect |
|
Preset Value |
DCONverter |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "DCONverter"
SCPI.SENSe.DCONverter.INPut = Var
Var = SCPI.SENSe.DCONverter.INPut
PN Menu: Input Port > Downconverter > RF Input
SP Menu: Input Port > Downconverter > RF Input
FP Menu: Input Port > Downconverter > RF Input
TR Menu: Input Port > Downconverter > RF Input
AM Menu: Input Port > Downconverter > RF Input
BB Menu: Input Port > Downconverter > RF Input
USER Menu: Input Port > Downconverter > RF Input
:SENSe:DCONverter:INPut {DCONverter|DIRect}
:SENSe:DCONverter:INPut?
{DCONverter|DIRect} <newline><^END>
10 OUTPUT 717;":SENSe:DCONverter:INPut DCONverter"
20 OUTPUT 717;":SENSe:DCONverter:INPut ?"
30 ENTER 717;A$