Property (Read-Write)
SCPI.SENSe.DCONverter.MEXTernal = Value
Value = SCPI.SENSe.DCONverter.MEXTernal
This command sets/gets external mixer selection.
|
Parameter |
Value |
|
Description |
External mixer selection |
|
Data Type |
Character string type (String) |
|
Range |
OFF|ON |
|
Preset Value |
OFF |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "OFF"
SCPI.SENSe.DCONverter.MEXTernal = Var
Var = SCPI.SENSe.DCONverter.MEXTernal
PN Menu: Input Port > Downconverter > External Mixer
SP Menu: Input Port > Downconverter > External Mixer
FP Menu: Input Port > Downconverter > External Mixer
TR Menu: Input Port > Downconverter > External Mixer
AM Menu: Input Port > Downconverter > External Mixer
BB Menu: Input Port > Downconverter > External Mixer
USER Menu: Input Port > Downconverter > External Mixer
:SENSe:DCONverter:MEXTernal {OFF|ON}
:SENSe:DCONverter:MEXTernal?
{OFF|ON} <newline><^END>
10 OUTPUT 717;":SENSe:DCONverter:MEXTernal OFF"
20 OUTPUT 717;":SENSe:DCONverter:MEXTernal ?"
30 ENTER 717;A$