SCPI.SENSe.FP(Ch).DCONverter.SSEarch.EXECute

Object Type

Method (Write Only)

Syntax

SCPI.SENSe.FP(Ch).DCONverter.SSEarch.EXECute

Description

This command searches carrier signal, for the selected channel Ch.

Examples

SCPI.SENSe.FP1.DCONverter.SSEarch.EXECute

Equivalent Key

No equivalent key is available on the front panel.

Equivalent SCPI Command

Syntax

:SENSe:FP[1-1]:DCONverter:SSEarch:EXECute

Example of use

10 OUTPUT 717;":SENSe:FP1:DCONverter:SSEarch:EXECute"