SCPI.SENSe.PN(Ch).ASET

Object Type

Method (Write Only)

Syntax

SCPI.SENSe.PN(Ch).ASET

Description

This command sets Attn, Freq Band and IF Gain Auto Set, for the selected channel Ch.

Examples

SCPI.SENSe.PN1.ASET

Equivalent Key

No equivalent key is available on the front panel.

Equivalent SCPI Command

Syntax

:SENSe:PN[1-1]:ASET

Example of use

10 OUTPUT 717;":SENSe:PN1:ASET"