Property (Read Only)
Value = SCPI.SENSe.SP(Ch).SWEep.POINts
This command gets number of points, for the selected channel Ch.
|
Parameter |
Value |
|
Description |
Number of points |
|
Data Type |
Long integer type (Long) |
|
Range |
2 ~ 1024 |
|
Preset Value |
154 |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
No |
|
Save-Recall Effect |
No |
|
Error |
- |
Dim Var as Long
Var= 2
Var = SCPI.SENSe.SP1.SWEep.POINts
No equivalent key is available on the front panel.
:SENSe:SP[1-1]:SWEep:POINts?
{2 ~ 1024} <newline><^END>
10 OUTPUT 717;":SENSe:SP1:SWEep:POINts ?"
20 ENTER 717;A