SCPI.SYSTem.PERSona.DEFault

Object type

Method (Write Only)

Syntax

SCPI.SYSTem.PERSona.DEFault

Description

This command reverts both manufacturer name and model number to the default.

Examples

SCPI.SYSTem.PERSona.DEFault

Related objects

SCPI.SYSTem.PERSona.MANufacturer.DEFault

SCPI.SYSTem.PERSona.MODel.DEFault

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:SYSTem:PERSona:DEFault

Query response

None

Example of use

10 OUTPUT 717;":SYST:PERS:DEF"