SCPI.SYSTem.PRESet

Object Type

Method (Write Only)

Syntax

SCPI.SYSTem.PRESet

Description

This command sets preset instrument state. It is same as: '*RST;:INIT:instr:CONT ON'(`instr' is all instrument)..

Examples

SCPI.SYSTem.PRESet

Equivalent Key

No equivalent key is available on the front panel.

Equivalent SCPI Command

Syntax

:SYSTem:PRESet

Example of use

10 OUTPUT 717;":SYSTem:PRESet"