SCPI.SYSTem.SET

Object Type

Method (Write Only)

Syntax

SCPI.SYSTem.SET

Description

This command sets the instrument to the state determined by the contents of the parameter.

Examples

SCPI.SYSTem.SET

Equivalent Key

No equivalent key is available on the front panel.

Equivalent SCPI Command

Syntax

:SYSTem:SET

Example of use

10 OUTPUT 717;":SYSTem:SET NONE"