Property (Read-Write)
SCPI.TRIGger.FP(Ch).MODE = Value
Value = SCPI.TRIGger.FP(Ch).MODE
This command sets/gets trigger mode, for the selected channel Ch.
|
Parameter |
Value |
|
Description |
Trigger mode |
|
Data Type |
Character string type (String) |
|
Range |
ANALyzer|TESTer |
|
Preset Value |
ANALyzer |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
100, "Option not installed" |
Dim Var as String
Var= "ANALyzer"
SCPI.TRIGger.FP1.MODE = Var
Var = SCPI.TRIGger.FP1.MODE
FP Menu: Trigger > Mode
:TRIGger:FP[1-1]:MODE {ANALyzer|TESTer}
:TRIGger:FP[1-1]:MODE?
{ANALyzer|TESTer} <newline><^END>
10 OUTPUT 717;":TRIGger:FP1:MODE ANALyzer"
20 OUTPUT 717;":TRIGger:FP1:MODE ?"
30 ENTER 717;A$