Property (Read-Write)
SCPI.TRIGger.PN(Ch).SOURce = Value
Value = SCPI.TRIGger.PN(Ch).SOURce
This command sets/gets trigger source, for the selected channel Ch.
|
Parameter |
Value |
|
Description |
Trigger source |
|
Data Type |
Character string type (String) |
|
Range |
INTernal|EXTernal|MANual|BUS |
|
Preset Value |
INTernal |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "INTernal"
SCPI.TRIGger.PN1.SOURce = Var
Var = SCPI.TRIGger.PN1.SOURce
PN Menu: Trigger > Source
:TRIGger:PN[1-1]:SOURce {INTernal|EXTernal|MANual|BUS}
:TRIGger:PN[1-1]:SOURce?
{INTernal|EXTernal|MANual|BUS} <newline><^END>
10 OUTPUT 717;":TRIGger:PN1:SOURce INTernal"
20 OUTPUT 717;":TRIGger:PN1:SOURce ?"
30 ENTER 717;A$