Property (Read-Write)
SCPI.TRIGger.TR(Ch).SOURce = Value
Value = SCPI.TRIGger.TR(Ch).SOURce
This command sets/gets trigger source, for the selected channel Ch.
Sets N2Video automatically when the measurement mode changed from WN to NN if selected WVIDeo.
Sets WVIDeo automatically when the measurement mode changed form NN to WN if selected N2Video.
|
Parameter |
Value |
|
Description |
Trigger source |
|
Data Type |
Character string type (String) |
|
Range |
INTernal|EXTernal|MANual|BUS|WVIDeo|NVIDeo|N2Video |
|
Preset Value |
INTernal |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "INTernal"
SCPI.TRIGger.TR1.SOURce = Var
Var = SCPI.TRIGger.TR1.SOURce
TR Menu: Trigger > Source
:TRIGger:TR[1-1]:SOURce {INTernal|EXTernal|MANual|BUS|WVIDeo|NVIDeo|N2Video}
:TRIGger:TR[1-1]:SOURce?
{INTernal|EXTernal|MANual|BUS|WVIDeo|NVIDeo|N2Video} <newline><^END>
10 OUTPUT 717;":TRIGger:TR1:SOURce INTernal"
20 OUTPUT 717;":TRIGger:TR1:SOURce ?"
30 ENTER 717;A$