Questionable Status Condition Register

Bit Position

Name

Description

0

Not used

Always 0.

1

Questionable Current Status Register Summary

Set to “1” when one of the enable bits in questionable current status register is set to “1.”

2

Not used

Always 0.

3

Questionable Power Status Register Summary

Set to “1” when one of the enable bits in questionable power status register is set to “1.”

4

Not used

Always 0.

5

RF frequency out of range

Set to “1” when DUT’s oscillation frequency is out of E5052B’s measurement range. In this case, DUT’s oscillation frequency should be verified.

6

Questionable Phase Status Register Summary

Set to “1” when one of the enable bits in the questionable phase status register is set to “1.”

7-8

Not used

Always 0.

9

Questionable Limit Status Register Summary

Set to “1” when one of the enable bits in the questionable limit status register is set to “1.”

10

Questionable Reference Signal Status Register Summary

Set to “1” when one of the enable bits in the questionable reference signal status register is set to “1.”

11

Questionable Misc Status Register Summary

Set to “1” when one of the enable bits in the questionable misc. status register is set to “1.”

12

Power-on Test FAIL

Set to “1” when the power-on self test results in “FAIL.”

13-15

Not used

Always 0.