You can operate the E5052B using one of three operating methods: using keys on the front panel, using a mouse and keyboard, and using the touch screen.
In the next section and those following it, a series of operations is expressed as follows:
Select Meas/View > Phase Noise > Window Max > Avg/BW

Press the Meas/View key in the Measurement Block.
Press
or
key to move the cursor to Phase Noise, then press Enter or (
) key.
Press Avg/BW

From the PN Menu click Measurement View, click Phase Noise and then click Return
Click Average
Press Measurement View > Phase Noise
Press Show Window and set all windows except Phase Noise to OFF status and then press Return.

Press Return to get back to PN menu.
Press Average