This section describes the process to evaluate different parameters of a VCO (Voltage Controlled Oscillator) using the E5052B. The VCO used for this example has the following specification:
|
Parameter |
Value |
|
Vcc (Bias Voltage) |
5 ± 0.5 V |
|
Vt (Tuning Voltage) |
+1.0 ~ +4.5V |
|
RF Output |
800 ± 30 MHz |
Preset the E5052B to factory settings by Preset > Factory.
Set DUT (VCO) Bias Voltage (Vcc) Settings by DC Power:
Set Min Pwr Voltage Limit as 4.5 V (3 in the figure below).
Set Max Pwr Voltage Limit as 5.5 V (4 in the figure below).
Set DC Power Delay as 100ms (5 in the figure below).
Set DC Power Voltage as 5V (2 in the figure below).

Set DUT (VCO) Tuning Voltage (Vt) Settings by DC Control:
Set Min Ctrl Voltage Limit as 1.0 V (3 in the figure below).
Set Max Ctrl Voltage Limit as 4.5 V (4 in the figure below).
Set DC Control Delay as 100ms (5 in the figure below).
Set DC Control Voltage as 1V (2 in the figure below).

Connect DUT to E5052B.

Set DC Power > DC Power Output ON
Set DC Control > DC Control Output ON
Set Display > Update
Phase Noise
Measurement
Press Meas/View > Phase Noise to activate Phase Noise window. Press Window Max to maximize the window
Press Setup > Frequency Band > 250M-7GHz
Press Trigger > Trigger to Phase Noise > Continuous to start measurements
Press Start/Center (Stop/Span), set Start > 100Hz and Stop > 40MHz
Press Attn > Input Attenuator 0dB for best dynamic range. Press Entry Off to clear the warning message that appears at bottom left
Press Avg/BW > Avg factor 8 > Averaging > ON to reduce fluctuation
Press Scale > Auto Scale
If the 1 GHz signal is a signal of a VCO, you can control the frequency of the signal by using the automatic frequency control (AFC) function.
Press DC Control > Auto Freq Control.
Set Target > 1GHz.
Set Tolerance > 10kHz.
Set Sensitivity > 10MHz/V.
Press AFC Status, then turn “ON” to activate AFC. When “AFC out of loop” message is displayed, change the value for tolerance or sensitivity to a value larger than the current setting.
C. Analysis Using Marker
Press Marker > Marker1 > 20 > x1 to check phase noise at 20MHz offset

Spectrum Monitor
Measurement
Press Meas/View > Spectrum Monitor to activate Spectrum window.
Press Window Max to maximize the window.
Press Trigger > Trigger to Spectrum Monitor > Continuous to start measurements
Press Start/Center (Stop/Span), set Center to carrier frequency displayed in phase noise window.
Press Setup > Reference Level > 5dBm to specify maximum input level of the measurement signal that is input from the RF IN port.
Press Scale > Auto Scale
Analysis Using Marker
Press Marker Search > Search Max

Frequency and Power
Measurement
Press Meas/View > Freq & Power to activate Frequency and Power window. Press Window Max to maximize the window
Press Setup > Frequency Band > 250M-7GHz
Tester Mode
Press Setup > Frequency Resolution > 10Hz
Press Trigger > Mode > Tester
Press Trigger > Trigger to Freq & Power > Continuous to start measurements

Analyzer Mode
Press Trigger > Mode > Analyzer
Press Setup > Sweep Parameter > Control Voltage
Press Setup > Frequency Resolution > 10Hz
Press Setup > Points > 51 to perform tuning selectivity measurement
Press Start/Center (Stop/Span) > DC Control Start 1V > DC Control Stop 4.5V
Press Scale > Auto Scale All
Press Setup > Sweep Parameter > Power Voltage to perform frequency pushing measurement
Press Start/Center (Stop/Span) > DC Power Start 4.5V > DC Power Stop 5.5V
Press Scale > Auto Scale All
Using touch screen touch Frequency screen to activate. Press Format > Frequency Format > Hz/V
Press Scale > Auto Scale All
Analysis Using Marker
Tuning Sensitivity
Press Marker > Marker1 > 1 > Enter
Press Marker > Marker2 > 1.5 > Enter
Press Marker > Marker3 > 2 > Enter
Press Marker > Marker4 > 2.5 > Enter
Press Marker > Marker5 > 3 > Enter
Press Trace Next to select Power trace in Frequency and Power window and repeat steps 1 to 5.
Press Trace Next to select Current trace in Frequency and Power window and repeat steps 1 to 5.
Press Trace Next to select Freq trace in Frequency and Power window and repeat steps 1 to 5.

Frequency Pushing
Press Marker > Marker1 > 4.5 > Enter
Press Marker > Marker2 > 4.7 > Enter
Press Marker > Marker3 > 5 > Enter
Press Trace Next to select Power trace in Frequency and Power window and repeat steps 1 to 3.
Press Trace Next to select Current trace in Frequency and Power window and repeat steps 1 to 3.
Press Trace Next to select Freq trace in Frequency and Power window and repeat steps 1 to 3.

AM Noise Measurement
Measurement
Press Meas/View > AM Noise to activate AM Noise window. Press Window Max to maximize the window
Press Setup > Frequency Band > 250M-7GHz
Press Trigger > Trigger to AM Noise > Continuous to start measurements
Press Start/Center (Stop/Span), set Start > 100Hz and Stop > 40MHz
Press Attn > Input Attenuator 0dB for best dynamic range. Press Entry Off to clear the warning message that appears at bottom left
Press Avg/BW > Avg factor 8 > Averaging > ON to reduce fluctuation
Press Scale > Auto Scale
Analysis Using Marker
Press Marker > Marker1 > 100 > x1
Press Marker > Marker2 > 1 > k/m
Press Marker > Marker3 > 1 > M/μ
Press Marker > Marker4 > 40 > M/μ