Only the Main Cal commands corresponding to the Phase Noise measurement class are documented here. All other commands are identical to the Cal commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtabs on the graphic below.
Click here to view links to Cal commands for all Measurement Classes.
| Main Tab Commands | |||
Softkey |
Sub-item | SCPI |
COM |
|
|
||
|
|||
| Src Power Correct | ON/OFF | SOURce:POWer:CORRection[:STATe] | SourcePowerCorrection |
| Interpolation | ON/OFF | SENSe:CORRection:INTerpolate[:STATe] | InterpolateCorrection |
| Correction Methods... |
|
||
| Correction Properties... | None | Properties |
|