CALCulate:MEASure:BLIMit Commands

These commands are for setting up bandwidth tests.

CALCulate:MEASure:BLIMit

BWIDth

       | THReshold

DISPlay

       | MARKer

             | STATe

FAIL?

MAXimum

MINimum

REPort

       | DATA?

[:STATe]

Click a keyword to view the command details.

See Also


CALCulate<cnum>:MEASure<mnum>:BLIMit:BWIDth:THReshold <value>

Applicable Models: All

(Read-Write) Sets bandwidth threshold value (attenuation from the peak) of the bandwidth test.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<value>

Bandwidth N dB points

Examples

CALC:MEAS:BLIM:BWID:THR 5
calculate2:measure2:blimit:display:bwidth:threshold 5

Query Syntax

CALCulate<cnum>:MEASure<mnum>:BLIMit:BWIDth:THReshold?

Return Type

Numeric

Default

3


CALCulate<cnum>:MEASure<mnum>:BLIMit:DISPlay:MARKer:STATe <bool>

Applicable Models: All

(Read-Write) Turns ON/OFF the bandwidth value display of the bandwidth test, for the active trace of selected channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<bool>

ON or 1 - Turns limit testing ON.
OFF or 0
- Turns limit testing OFF.

Examples

CALC:MEAS:BLIM:DISP:MARK:STAT ON
calculate2:measure2:blimit:display:marker:state off

Query Syntax

CALCulate<cnum>:MEASure<mnum>:BLIMit:DISPLay:BWIDth:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:MEASure<mnum>:BLIMit:FAIL?

Applicable Models: All

(Read-only) Get the bandwidth limit test results, for the active trace of selected channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<bool>

Boolean

  • 0 is returned when Pass

  • 1 is returned when Fail

Examples

CALC:MEAS:BLIM:FAIL?
calculate2:measure2:blimit:fail?

Query Syntax

CALCulate<cnum>:MEASure<mnum>:BLIMit:FAIL?

Return Type

Boolean

Default

Not Applicable


CALCulate<cnum>:MEASure<mnum>:BLIMit:MAXimum <max>

Applicable Models: All

(Read-Write) Sets/gets the upper limit value of the bandwidth test, for the selected channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<max>

Maximum bandwidth

Examples

CALC:MEAS:BLIM:MAX 1E6
calculate2:measure2:blimit:maximum 1E6

Query Syntax

CALCulate<cnum>:MEASure<mnum>:BLIMit:MAXimum?

Return Type

Numeric

Default

300000


CALCulate<cnum>:MEASure<mnum>:BLIMit:MINimum <min>

Applicable Models: All

(Read-Write) Sets or returns the lower limit value of the bandwidth test, for the selected channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<min>

Minimum bandwidth

Examples

CALC:MEAS:BLIM:MIN 1E6
calculate2:measure2:blimit:minimum 1E6

Query Syntax

CALCulate<cnum>:MEASure<mnum>:BLIMit:MINimum?

Return Type

Numeric

Default

10000


CALCulate<cnum>:MEASure<mnum>:BLIMit:REPort:DATA?

Applicable Models: All

(Read-only) Read the bandwidth value of the bandwidth test, for the active trace of selected channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

Examples

CALC:MEAS:BLIM:REP:DATA?
calculate2:measure2:blimit:report:data?

Query Syntax

CALCulate<cnum>:MEASure<mnum>:BLIMit:REPort:DATA?

Return Type

Numeric

Default

OFF


CALCulate<cnum>:MEASure<mnum>:BLIMit[:STATe]

Applicable Models: All

(Read-Write) Turns ON/OFF the bandwidth test function, for the active trace of selected channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<bool>

ON or 1 - Turns limit testing ON.
OFF or 0
- Turns limit testing OFF.

Examples

CALC:MEAS:LIM:STAT ON
calculate2:measure2:limit:state off

Query Syntax

CALCulate<cnum>:MEASure<mnum>:BLIMit:DIPLay:MARKer:STATe?

Return Type

Boolean

Default

OFF