Controls the limit segments used for pass / fail testing.
CALCulate:MEASure:LIMit | DELete DISPlay | [:STATe] REPort | ALL? | [:DATA]? | POINts? SEGMent | AMPLitude | STARt | STOP | COUNt? | STIMulus | STARt | STOP | TYPE SOUNd | [:STATe] |
Click a keyword to view the command details.
See Also
Applicable Models: All (Read-Write) Sets data for limit segments. |
|||||||||||
Parameters |
|
||||||||||
<cnum> |
Channel number of the measurement (optional). |
||||||||||
<mnum> |
Measurement number for each measurement. |
||||||||||
<block> |
Data
for all limit segments. The following is the data format for 1
segment:
|
||||||||||
Examples |
The following writes three max limit segments for a bandpass filter. CALC:MEAS2:LIM:DATA 1,3e5,4e9,-60,0,1,4e9,7.5e9,0,0,1,7.5e9,9e9,0,-30 |
||||||||||
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:DATA? |
||||||||||
Return Type |
Depends on FORM:DATA |
||||||||||
Maximum limit = 100 |
|||||||||||
Applicable Models: All (Write-only) Deletes all limit line data for the selected measurement on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC2:MEAS2:LIM:DATA:DEL |
Query Syntax |
Not Applicable |
Not Applicable |
|
Applicable Models: All (Read-Write) Turns the display of limit segments ON or OFF (if the data trace is turned ON). |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<ON | OFF> |
ON
(or 1) - turns the display
of limit segments ON. |
Examples |
CALC:MEAS2:LIM:DISP:STAT
ON |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:DISPlay[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
ON |
|
Applicable Models: All (Read-only) Returns the Pass / Fail status of the limit line test. Returns 1 (Fail) if any data point fails for any limit segment. Limit display (CALC:LIM:DISP) does NOT have to be ON. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS2LIM:FAIL? |
Return Type |
Boolean
|
Not Applicable |
|
Applicable Models: All (Read-only) Returns the test results (stimulus value, limit test result, upper limit value and lower limit value of all measurement points), for the selected trace. This command returns a point by point description of the limit table and pass/fail test result. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<block> |
Depends on FORM:DATA If the number of the measurement points is N, <Block> = <first stimulus>,<test result>,<upper limit>,<lower limit>, …, <Nth stimulus>,<test result>,<upper limit>,<lower limit> Where <test result>= -1: No limit, 0:Fail, 1:Pass |
Examples |
The following example returns three points: CALC:MEAS2:LIM:REP:ALL? +1.00000000000E+009, 'bucket 1 XAxis value +1.00000000000E+000, 'result (1 == Pass) -4.90000009537E+000, 'upper limit -5.05000019073E+000, 'lower limit
+3.00000000000E+009, 'bucket 2 XAxis value +1.00000000000E+000, -4.84999990463E+000, -5.19999980927E+000,
+5.00000000000E+009, 'bucket 3 Xaxis value -1.00000000000E+000, +0.00000000000E+000, +0.00000000000E+000 |
Return Type |
Variant |
Depend on the preset status |
|
Applicable Models: All (Read-only) Returns the stimulus values (frequency, power level or time) at all the measurement points that failed the limit test, for the selected trace. If there are no failures, a large number is returned (+9.91000000000E+037). |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<block> |
Depends on FORM:DATA If the number of the measurement points that failed the limit test is N, <block>=<First failed stimulus>, ..., <Nth failed stimulus>. |
Examples |
The following example assumes that there are no failures: CALC:MEAS2:LIM:REP:DATA? +9.91000000000E+037 |
Return Type |
Numeric |
9.91E37 (no failures) |
|
Applicable Models: All (Read-only) Reads the number of the measurement points that failed the limit test, for the active trace of selected channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS:LIM:REP:POIN? |
Query Syntax |
Numeric |
0 |
|
Applicable Models: All (Read-Write) Sets the start (beginning) of the Y-axis amplitude (response) value. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<snum> |
Segment number; if unspecified, value is set to 1. |
<num> |
Choose any number between: -500 and 500 Display value is limited to the Maximum and Minimum displayed Y-axis values. |
Examples |
CALC:MEAS2LIM:SEGM1:AMPL:STAR
10 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>AMPLitude:STARt? |
Return Type |
Numeric |
0 |
|
Applicable Models: All (Read-Write) Sets the stop (end) of the Y-axis amplitude (response) value. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<snum> |
Segment number; if unspecified, value is set to 1. |
<num> |
Choose any number between: -500 and 500 Display value is limited to the Maximum and Minimum displayed Y-axis values. |
Examples |
CALC:MEAS:LIM:SEGM1:AMPL:STOP
10 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>AMPLitude:STOP? |
Return Type |
Numeric |
0 |
|
Applicable Models: All (Read-only) Returns the number of segments used in a limit test. All segments are counted, whether they are on or not. |
|
Parameters |
Not Applicable |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS2:LIM:SEGM:COUN? |
Return Type |
Numeric |
Not Applicable |
|
Applicable Models: All (Read-Write) Sets the start (beginning) of the X-axis stimulus value. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<snum> |
Segment number; if unspecified, value is set to 1. |
<num> |
Choose any number within the X-axis span of the analyzer. |
Examples |
CALC:MEAS:LIM:SEGM1:STIM:STAR
10 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>STIMulus:STARt? |
Return Type |
Numeric |
0 |
|
Applicable Models: All (Read-Write) Sets the stop (end) of the X-axis stimulus value. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<snum> |
Segment number; if unspecified, value is set to 1. |
<num> |
Choose any number within the X-axis span of the analyzer. |
Examples |
CALC:MEAS2:LIM:SEGM1:AMPL:STOP
10 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>STIMulus:STOP? |
Return Type |
Numeric |
0 |
|
Applicable Models: All (Read-Write) Sets the type of limit segment. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<snum> |
Segment
number. Choose any number between: |
<char> |
Choose from: LMIN - a MIN limit segment. Any response data below the MIN value will fail. OFF - the limit segment (display and testing) is turned OFF. |
Examples |
CALC:MEAS2:LIM:SEGM:TYPE
LMIN |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>:TYPE? |
Return Type |
Character |
OFF |
|
Applicable Models: All (Read-Write) Turns limit testing fail sound ON or OFF. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<ON | OFF> |
ON
(or 1) - turns sound ON. |
Examples |
CALC:MEAS2:LIM:SOUN
ON |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SOUNd[:STATe]? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
|
Applicable Models: All (Read-Write) Turns limit segment testing ON or OFF.
|
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<ON | OFF> |
ON
(or 1) - turns limit testing
ON. |
Examples |
CALC:MEAS:LIM:STAT
ON |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:STATe? |
Return Type |
Boolean (1 = ON, 0 = OFF) |
OFF |
|