CALCulate:MEASure:SMOothing Commands

Controls point-to-point smoothing. Smoothing is a noise reduction technique that averages adjacent data points in a measurement trace. Choose the amount of smoothing by specifying either the number of points or the aperture. Smoothing is not the same as CALC:AVERage which averages each data point over a number of sweeps.

CALCulate:MEASure:SMOothing

APERture

POINts

[:STATe]

Click a keyword to view the command details.

See Also


CALCulate<cnum>:MEASure<mnum>:SMOothing:APERture <num>

Applicable Models: All

(Read-Write) Sets the amount of smoothing as a percentage of the number of data points in the channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<num>

Percentage value. Choose any number between:
1
and 25

Examples

CALC:MEAS:SMO:APER 2
calculate2:measure2:smoothing:aperture 20.7

Query Syntax

CALCulate<cnum>:MEASure<mnum>:SMOothing:APERture?

Return Type

Numeric

Default

1


CALCulate<cnum>:MEASure<mnum>:SMOothing:POINts <num>

Applicable Models: All

(Read-Write) Sets the number of adjacent data points to average.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<num>

Number of points from 1 point to maximum of 25% of data points in the channel. For example: if number of points in a data trace = 401, the maximum value for points = 100. The points value is always rounded to the closest odd number.

Examples

CALC:MEAS:SMO:POIN 50
calculate2:measure2:smoothing:points 21

Query Syntax

CALCulate<cnum>:MEAsure<mnum>:SMOothing:POINts?

Return Type

Numeric

Default

3


CALCulate<cnum>:MEASure<mnum>:SMOothing[:STATe] <bool>

Applicable Models: All

(Read-Write) Turns data smoothing ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<bool>

ON or 1 - Turns smoothing ON.
OFF or 0
- Turns smoothing OFF.

Examples

CALC:MEAS:SMO ON
calculate2:measure2:smoothing:state off

Query Syntax

CALCulate<cnum>:MEASure<mnum>:SMOothing[:STATe]

Return Type

Boolean (1 = ON, 0 = OFF)

Default

OFF