Controls the display of Y-axis for various measurements.
CALCulate:MEASure:Y AXIS | UNIT? | CUSTom | DATA |
Click a keyword to view the command details.
See Also
Applicable Models: All (Read-only) Returns the current units of the Y-axis (HZ | SECond | MINute | HOUR | DAY | DB | DBM | DBMV | WATTs | FARad | HENRy | OHM | MHO | SIEMen | VOLT | DEGRee | RADians | METer | DPHZ | UNIT | NONe | TNORmalized | NTEMperature | KELVin|CENTigrade | FAHRenheit | FEET | INCH | DBMAAMPere | VOLTAge | DBUV | PERCentage | DMVRoothz | DUVRoothz | DMARoothz | WPHZ | VROothz | AROothz | DBC | DVPerhz | DCPerhz | DBPerhz | HZPerhz | PRHz | VPHz | DBV|DEFault). This command can be used for all Measurement Classes. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS2:Y:AXIS:UNIT? |
Return Type |
Enumeration |
FREQuency |
|
Applicable Models: All (Write-Read) Set and query y axis unit. This command can be used for all Measurement Classes. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<string> |
any unit in string |
Examples |
CALC:MEAS2:Y:AXIS:UNIT:CUST:DATA "U" |
Query Syntax |
CALCulate:MEASure:Y:AXIS:UNIT:CUSTom:DATA? |
Return Type |
String |
"" |
|
Applicable Models: All (Write-Read) Set and query the state of Y axis unit This function is used to display the user specific Y axis unit. This command can be used for all Measurement Classes. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<bool> |
ON (or 1) - Y axis unit is the string specified by CALC:MEAS:Y:AXIS:UNIT:CUSTom:DATA OFF (or 0) - Y axis unit is the default of each measurement parameter (depends on trace format) |
Examples |
CALC:MEAS2:Y:AXIS:UNIT:CUST:STAT ON |
Query Syntax |
CALCulate:MEASure:Y:AXIS:UNIT:CUSTom:STATe? |
Return Type |
Boolean |
OFF (0) |
|
Applicable Models: All (Read-only) Returns the Y-axis values for the selected measurement in the current units. This command can be used for all Measurement Classes. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS2:Y? |
Return Type |
Array of data |
Not applicable |
|