Sense User (User Commands)

Define the settings for User Display measurement class.

SENSe:USER

| X

| AXIS

| SPACing

| UNIT

| [:VALues]

 

 

 


SENSe<cnum>:USER:X:AXIS:SPACing <Enum>

Applicable Models: E505xA

(Read-Write) Set and query x-axis spacing. This property is used to determine the scale of x-axis and interpolation method of marker etc..

Parameters

 

<Enum>

Choose from:

LIN - LINear

LOG - LOGarithmic

Examples

SENS:USER:X:AXIS:SPAC LOG

sense:user:x:axis:spacing log

Query Syntax

SENSe:USER:X:AXIS:SPACing?

Return Type

Enum

Default

LINear


SENSe<cnum>:USER:X:AXIS:UNIT <string>

Applicable Models: E505xA

(Read-Write) Set and query x-axis unit.

Parameters

 

<string>

any unit in string

Examples

SENS:USER:X:AXIS:UNIT "m"

sense:user:x:axis:unit "m"

Query Syntax

SENSe:USER:X:AXIS:UNIT?

Return Type

String

Default

"U"


SENSe<cnum>:USER:X[:VALues] <data>

Applicable Models: E505xA

(Read-Write) Set and query x-axis data and number of points.

Use FORMat:DATA to change the data type. (<REAL,32>, <REAL,64> or <ASCii,0>)

Parameters

 

<data>

Arbitrary data array with ascending order

Examples

SENS:USER:X:VAL 30,40,50,60,70,80

sense:user:x:values 30,40,50,60,70,80

Query Syntax

SENSe:USER:X:VALues?

Return Type

Data type specified by FORMat:DATA

Default

<10,20,30,40,50,60,70,80,90,100>