System Service SCPI


Controls and queries for programmatically interacting with the PathWave Calibration Advisor software application.

SYSTem:SERVice:

MANagement

       | CALibration

                | INFormation?

                | INTerval

                     | DEFault

                     | TYPE?

                     | [:VALue]

                | NOTification

                     | ENABle

                | PASScode

                     | CHANge

                     | [:VALue]

                | PERiodic

                     | ENABle

                | REMinder

 

Click on a red keyword to view the command details.

See Also


SYSTem:SERVice:MANagement:CALibration:INFormation?

Applicable Models: All

(Read only) Returns the instrument calibration information in JSON format. The returned value includes the following:

  • CalID – Calibration ID number created by the service center when the instrument was calibrated.

  • CalBy – Service center that calibrated this instrument – either "Keysight Technologies" or "Keysight Authorized Calibration Provider".

  • CalDate – Date of last calibration.

  • CalDueDate – Calibration due date. The due date is calculated as CalDate + Calibration Interval, unless a shelf life policy is applied.

  • Status – returned value depends on:

    • If SystemTime≤CalDueDate, Status is "CalibrationValid".

    • If SystemTime>CalDueDate, Status is "CalibrationRequired".

    • If CalDueDate is empty, and CalDate is presented, Status is "CalibrationValid".

    • If SystemTime<CalDate, Status is "CalibrationUnknown".

    • If Cal Data is unavailable, Status is "CalibrationNotFound".

  • SystemTime – Current system time.

Parameters

None

Examples

SYSTem:SERVice:MANagement:CALibration:INFormation?

'returns this format:

{"CalId":"1-00000000000-1","CalBy":"Keysight Technologies","CalDate":"27-May-2020","CalDueDate":"27-May-2021","Status":"CalibrationValid","SystemTime":"2020-11-18 10:38:08"}

Return Type

String of JSON format including all calibration info

Default

Not Applicable


SYSTem:SERVice:MANagement:CALibration:INTerval:DEFault

Applicable Models: All

(Write-only) Sets calibration interval to Keysight Recommended (according to the instrument model).

Parameters

None

Examples

SYST:SERV:MAN:CAL:INT:DEF

Query Syntax

Not Applicable

Default

Not Applicable


SYSTem:SERVice:MANagement:CALibration:INTerval:TYPE?

Applicable Models: All

(Read only) Returns the instrument calibration interval type. Three types may return:

  • DEFault: When current calibration interval is "Keysight recommended", the returned value is DEFault.
  • CUSTomer: When the current calibration interval is "user defined", the returned value is CUSTomer.
  • EMPTY: After new calibration info is imported and the calibration interval is not confirmed, the returned value is empty.

Parameters

None

Examples

SYSTem:SERVice:MANagement:CALibration:INTerval:TYPE?

CUSTomer

Return Type

Enum

Default

Not Applicable


SYSTem:SERVice:MANagement:CALibration:INTerval[:VALue] <value>

Applicable Models: All

(Read-Write) Sets and returns the calibration interval value (interval in months).

Notes:

  • If using this command to set to the calibration interval, the calibration interval type will be switched to user defined (CUSTomer).

  • This command only returns the value of current saved calibration interval type. Any unsaved changes will not be returned.

Parameters

 

<value>

Calibration interval in months. An integer between 1 and 120.

Examples

SYSTem:SERVice:MANagement:CALibration:INTerval:VALue 12

Query Syntax

SYSTem:SERVice:MANagement:CALibration:INTerval[:VALue]?

Return Type

Numeric

Default

Not Applicable


SYSTem:SERVice:MANagement:CALibration:NOTification:ENABle <bool>

Applicable Models: All

(Read-Write) Sets and returns the calibration status/due popup notification state during instrument running. If disabled, the notification will pop up only on power up. If enabled, the notification will also pop up at 12:00 AM every day when the current date is ≤ the Cal Due Reminder days set by SYSTem:SERVice:MANagement:CALibration:REMinder.

Parameters

 

<bool>

OFF (or 0): Popup notification is NOT visible while the instrument is running.
ON (or 1)
: Popup notification is visible while the instrument is running.

Examples

SYSTem:SERVice:MANagement:CALibration:NOTification:ENABle 0
SYSTem:SERVice:MANagement:CALibration:NOTification:ENABle OFF

Query Syntax

SYSTem:SERVice:MANagement:CALibration:NOTification:ENABle?

Return Type

Boolean

Default

1


SYSTem:SERVice:MANagement:CALibration:PASScode:CHANge <value>

Applicable Models: All

(Write-only) Sets new passcode.

Parameters

 

<value>

Passcode.
Requirements: 6-10 characters, limited to alpha (a-Z) and numeric (0-9) characters.

Examples

SYSTem:SERVice:MANagement:CALibration:PASScode:CHANge '1q2w3e4r'

Query Syntax

Not Applicable

Default

Not Applicable


SYSTem:SERVice:MANagement:CALibration:PASScode[:VALue] <value>

Applicable Models: All

(Write-only) Input existing passcode and enable all setting features.

Parameters

 

<value>

Last saved passcode (see SYSTem:SERVice:MANagement:CALibration:PASScode:CHANge)

Examples

SYSTem:SERVice:MANagement:CALibration:PASScode '1q2w3e4r'

Query Syntax

Not Applicable

Default

Key4Cal


SYSTem:SERVice:MANagement:CALibration:PERiodic:ENABle <bool>

Applicable Models: All

(Read-Write) Sets and returns the periodic calibration state.

Parameters

 

<bool>

OFF (or 0): Periodic calibration is disabled.
ON (or 1)
: Periodic calibration is enabled.

Examples

SYSTem:SERVice:MANagement:CALibration:PERiodic:ENABle 0
SYSTem:SERVice:MANagement:CALibration:PERiodic:ENABle OFF

Query Syntax

SYSTem:SERVice:MANagement:CALibration:PERiodic:ENABle?

Return Type

Boolean

Default

1


SYSTem:SERVice:MANagement:CALibration:REMinder <value>

Applicable Models: All

(Read-Write) Sets and returns the calibration due reminder days (30, 15, or 7).

Parameters

 

<value>

Calibration due reminder in days. Only one number: 30, 15, or 7.

Examples

SYSTem:SERVice:MANagement:CALibration:REMinder 30

Query Syntax

SYSTem:SERVice:MANagement:CALibration:REMinder?

Return Type

Numeric

Default

30