This Visual Basic example shows you how to configure the PNA-X internal pulse generators and modulators to make wideband pulsed measurements in pulse profile mode using the PNA-X.
Visit the VNA website where you can download a free Wideband Pulsed Application that performs this measurement on the PNA-X.
See all SCPI Pulsed examples
|
Private Sub Form_Load() Dim app Dim scpi ' Create / Get the VNA application. Set app = CreateObject("AgilentPNA835x.Application") Set scpi = app.ScpiStringParser 'Preset the analyzer scpi.Execute ("*RST")
'Set BW to 5 MHz scpi.Execute ("SENS:BWID 5MHZ") 'Set sweep type to CW mode scpi.Execute ("SENS:SWE:TYPE CW") 'Delete S11 trace scpi.Execute ("DISP:WIND:TRAC1:DEL") 'Create S21 trace scpi.Execute ("CALC:PAR:DEF:EXT 'MyMeas',S21") scpi.Execute ("DISP:WIND:TRAC1:FEED 'MyMeas'") 'Set modulation source to Pulse1 scpi.Execute ("sens:path:conf:elem 'PulseModDrive','Pulse1'") 'Set power leveling mode to Openloop scpi.Execute ("sour:pow1:alc:mode open") 'Enable pulse modulator 1 scpi.Execute ("sens:path:conf:elem 'Src1Out1PulseModEnable','Enable'") 'Set clock of internal pulse generator to internal scpi.Execute ("sens:path:conf:elem 'PulseTrigInput','Internal'") 'Turn on Pulse0 scpi.Execute ("SENS:PULS0:STAT 1") 'Turn on Pulse1 scpi.Execute ("SENS:PULS1:STAT 1") 'Set pulse period to 1 ms scpi.Execute ("sens:puls:per .001") 'Set Pulse1 width to 10 us scpi.Execute ("sens:puls1:width 0.00001") 'Set Pulse1 delay to 8 us scpi.Execute ("sens:puls1:delay 0.000008") 'Set Pulse0 width to 1 us scpi.Execute ("sens:puls0:width 0.000001") 'Set Pulse0 delay to 400 ns scpi.Execute ("sens:puls0:delay 0.0000004") 'Set trigger scope to Channel scpi.Execute ("TRIG:SCOP CURRENT")
End Sub |