This VBScript program does the following:
Preset the VNA
Return active channel number and measurement string
Create a marker
Set X-axis value
Read X, Y-axis values
Set marker to trace Min
Read X, Y-axis values
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as Markers.vbs. Learn how to setup and run the macro.
See all Marker SCPI commands.
See Other SCPI Example Programs
Dim na, vi, ret Set na = CreateObject("AgilentPNA835x.Application") Set vi = na.ScpiStringParser 'Get Identification String from Analyzer ret=vi.Parse("*IDN?") msgbox ret 'Preset VNA ret=vi.Parse("SYST:PRES; *OPC?") 'Get Active Channel and Measurement chan = vi.Parse("SYST:ACT:CHAN?") meas = vi.Parse("SYST:ACT:MEAS?") 'Convert chan to a single number chan=CStr(CInt(chan)) 'Select Active Measurement vi.Parse "CALC" + chan + ":PAR:SEL " + meas 'Turn Marker 1 on and set X value to 1 GHz vi.Parse "CALC" + chan + ":MARK1:STAT ON" vi.Parse "CALC" + chan + ":MARK1:X 1e9" 'Get X and Y marker values x_val = vi.Parse("CALC" + chan + ":MARK1:X?") y_val = vi.Parse("CALC" + chan + ":MARK1:Y?") 'Display Marker Values msgbox "X Value = " + x_val + Chr(10) + "Y Value = " + y_val 'Use Marker 1 as a minimum search vi.Parse "CALC" + chan + ":MARK1:FUNC:EXEC MIN" 'Get X and Y marker values x_val = vi.Parse("CALC" + chan + ":MARK1:X?") y_val = vi.Parse("CALC" + chan + ":MARK1:Y?") 'Display Marker Values msgbox "X Value = " + x_val + Chr(10) + "Y Value = " + y_val |