This VBScript program polls for the completion of a sweep.
This VBScript (*.vbs) program can be run as a macro in the analyzer. To do this, copy the following code into a text editor file such as Notepad and save it on the analyzer hard drive as NewMeas.vbs. Learn how to setup and run the macro.
See Other SCPI Example Programs
sub SweepAndPoll Write "SYST:PRES" ' Preset Write "SENS:SWE:MODE HOLD" ' Put the channel into hold mode Write "*ESE 1" ' Turn on the *ESR? bit Write "*CLS" ' Clear any pending status Write "SENS:SWE:MODE SING" ' Initiate a sweep, but don't wait for complete Write "*OPC" ' Request notification on sweep complete done = 0 count = 0 while (done <> 1) Write "*ESR?" ' Check if sweep is complete done = Read() wscript.sleep 100 ' Wait for 100 ms wend wscript.echo "Sweep Completed" end Sub
' Infrastructure to setup the Write/Read functions dim LastReadBuffer Sub Write(command) LastReadBuffer = s.Execute(command) end sub
Function Read() Read = LastReadBuffer end function
' Setup and Call SweepAndPoll set app = CreateObject("Agilentpna835x.application") set s = app.scpistringparser SweepAndPoll
|