The SCPI command recorder allows you to get the corresponding SCPI commands from your front panel operation. It helps you to know the required commands without checking the command reference.
How to execute SCPI Recorder |
|
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
The following SCPI Recorder Panel is displayed.

|
Menu |
Commands |
Icon |
Description |
|
File |
Load File... |
|
Open the recording file with .vrec file extension |
|
Save File... |
|
Save the recording file with .vrec file extension. |
|
|
Export Sequence... |
- |
Export the SCPI command list in a text format |
|
|
Exit |
- |
Exit the SCPI command recorder application |
|
|
Edit |
Edit Command |
|
Edit the command cell |
|
Add Row |
|
Add a new row at the end of table |
|
|
Insert Row |
- |
Insert a new row above the active row |
|
|
Delete Row |
|
Delete the active low |
|
|
Move Up |
|
Move up the active row |
|
|
Move Down |
|
Move down the active row |
|
|
Delete Blank Command Rows |
- |
Delete the rows which are blank in SCPI command column |
|
|
Clear Record |
- |
Clear the table |
|
|
Control |
Record |
|
Start the recording |
|
Stop |
|
Stop the recording and show the recorded commands in the log table |
|
|
Play |
|
Play commands in the log table |
|
|
Cunning |
- |
When checked, a corresponding SCPI command is displayed on the message area during front panel operation. This function is available even when the recording is not turned on. |
The recorded commands are listed in the log table.
Table shows these three column
GUI: Operation method from the front panel
Operation: Operation from Softkey, Entry, Menu, Dialog and Hardkey
SCPI Command: Corresponding SCPI command
Not all operation sequence is supported for recording. The following table shows the supported operation and command. A blank is filled if the operation is supported but SCPI command is not supported.
|
GUI |
Operation |
SCPI Command |
|
Softkey |
Supported |
Supported |
|
Entry |
Supported |
Partially Supported |
|
Menu from Menu bar |
Supported |
Partially Supported |
|
Dialog |
Partially Supported |
Not Supported |
|
Hardkey |
Partially Supported (*1) |
Partially Supported (*1) |
|
Tool bar button |
Not Supported |
Not Supported |
|
Mouse (trace drag and drop, right-click menu and direct marker/trace operations) |
Not Supported |
Not Supported |
(*1) Only for preset, marker and search hardkeys which can directly execute a command.
As the softkey operation is fully supported, it is recommended to use softkey if both Softkey and Dialog box are available for the same operation.
For example, use Sweep > Main > Sweep Type to select Sweep Type instead of Sweep > Main > Sweep Setup... (dialog box).
Show the connection and current status such as Recording and Playing