Softkey display |
Function |
2-1(S21 S11) |
Measure between test ports 1 and 2. selecting port 1 as the output. |
1-2(S12 S22) |
Measure between test ports 2 and 1. selecting port 2 as the output. |
An asterisk (*) in the upper right of the softkey indicates that, if you select the test port and execute acquisition of the calibration coefficient (press Done), the existing calibration coefficient will be cleared.