Softkey |
Function |
2-1 (S21) |
Selects test port 2 (input) and test port 1 (output); Corresponds to the determination of S21 |
1-2 (S12) |
Selects test port 1 (input) and test port 2 (output); Corresponds to the determination of S12 |
An asterisk (*) in the upper right of the softkey indicates that the existing calibration coefficient will be cleared if you select the test port and execute acquisition of the calibration coefficient (clicking Done).