Partial Overwrite Calibration

Other topics about Advanced Calibration

Overview

The partial overwrite function is used to perform partial measurement after the execution of calibration, and it overwrites the calibration coefficients.

There are three types of calibration coefficients: Er, Es, Ed for reflection, Et for transmission, and Ex for isolation. If some of them do not provide satisfactory calibration, you can use this function to re-calculate the calibration coefficients by measuring an applicable standard only instead of measuring all the standards again.

Procedure

Follow these steps to execute the partial overwrite function. The example demonstrates re-calibration thru calibration only for exiting 2 port full calibration:

  1. Press Channel Next (or Channel Prev) to select the channel of which you already have performed full 2 port calibration.

  2. Press Cal >Calibrate > 2-Port Cal.

  3. Click Transmission.

  4. Make a thru connection between the ports 1 and 2.

  5. Click Port 1-2 Thru.

  6. Click Return.

  7. Click Overwrite to finish the re-calibration for the full 2-port calibration. At this point, the calibration coefficients are re-calculated with the new thru calibration and saved.

.