Changing Sweep Conditions

When the below conditions change:

When these conditions change, interpolation is executed. Error correction status symbol, C? is displayed at the channel status bar at the lower part of the window. This indicates that the changes in the conditions are within an acceptable range. At this point, calibration is advisable but not mandatory.

When the below conditions change:

When these conditions change and the sweep span is extended, the extrapolation is executed. Error correction status symbol, Hence C! is displayed at the channel status bar at the lower part of the window. This indicates that the changes in the conditions are far from the acceptable range. At this point, calibration is mandatory.

Changing Measurement Points

To change the number of measurement points, refer to Setting the measurement points.

Changing Sweep Parameter

To change the sweep parameter, refer to Setting the sweep parameter.