Measuring Other DUTs

If you measure another DUT of the same type and size as the one used in the previous measurement, start measurement with Connecting DUT to Test Fixture. If you use the same test fixture to measure a DUT of a different type and size, start measurement with calibration or fixture compensation. When using a different test fixture, start measurement with Connecting Test Fixture.

When measuring a DUT in the initial state after turning the power ON, start measurement with Setting Measurement Conditions.