Zero span can not be used.
Do not change frequency setting and number of points.
Do not use softkey (on the right side of screen) excepts Marker and Marker Search functions.
Do not change number of channel. This application uses the other channels other than channel 1 in order to calculate the parameters.
Do not change the number of trace other than 4.
Do not change sweep type from Lin Freq.
Do not turn on "Gating", "Fault Location", "SRL", "Conversion", "Time Domain", "Frequency Offset" and "Impedance analysis" functions.
Sweep restarts if setting is changed during sweep. When the average function is on, the averaging count may not be the same as the actual averaging.
When data entry bar is opened, you cannot input the value in GUI entry. Press Entry Off to close the data entry bar.
The cable, fixture and measurement environment influence measurement accuracy. If their influences are big, the measurement may have a big error or be impossible.
Only Single-end measurement is supported. Balanced measurement is not supported.
The outer conductor of coaxial connector on the analyzer ports is terminated with chassis ground.
This application calculates the result from the S-pamameter analysis. The specified Vin is not actually applied to the DUT and the physical load (Load R and X) is not connected.
If the specified values in GUI are too big or small, the application may not operate correctly.
If the calculation includes "divided by 0" or is impossible, the result, marker reading, and data in saved file may not be correct.
If each result is almost the same in Mode-2, the graph may not be displayed.
If result includes both + and - values or 0, the log-y scale may not work and graph may not be displayed.
3D data cannot be saved as trace data.
Save the analyzer setting before the application launch. Select State Only or State & Cal as Save Type. Select ALL for Channel/Trace setting.
When recalling a state file, press preset and recall the state file before this application launch.
"U" is displayed as the unit of trace due to analyzer unit display limitation.