A warning message is displayed in the instrument message/Warning area in the lower left part of the display against a gray background. Pushing a front panel key or executing :DISP:CCL command clears the message.
This message simply appears on the display, being not known to a remote environment such as a GPIB. This message is not displayed when another error (against a red background) is already displayed in the instrument message/Warning area.
|
Messages |
Description |
|
Calibration data lost ([parameter])/ |
One or more of the below calibration data is lost. The lost parameter is indicated in the message, for example, calibration data lost (band information): (nominal value), (band information), (frequency reference), (synthesizer gain), (source output power), (DC bias level), (mixer offset), (receiver IF range), (port characteristics), (gain phase ratio), (absolute gain), (distortion), (src dc offset), (constants for sweep controller) |
|
Invalid key code |
The key code entered to enable or disable an option is incorrect. Enter the correct key code to proceed. |
|
Load VBA project error |
This warning message is displayed when the attempt to upload a VBA project fails. Check the validity of the VBA project file. |
|
Peak not found |
This warning message is displayed when, with the tracking turned ON, the peak specified by the marker search has not been found by the time the sweep is finished (with the tracking executed). |
|
Target value not found |
This warning message is displayed when, with the tracking turned ON, the target specified by the marker search has not been found by the time the sweep is finished (with the tracking executed). This warning message is displayed also when, with the bandwidth marker displayed, the setting for the bandwidth marker is changed at the end of the sweep, or when, with the active marker changed or moved, the bandwidth is not found. |
|
Unable to find help file |
This warning message appears when Help file could not be executed when you press the Help key. The file is either corrupted or unavailable. |
|
Unable to find help id file |
This warning message appears when Help file could not be executed when you click a button at the menu bar and press the Help key to execute a help topic related to the button. The help id file is either corrupted or unavailable. |