Property (Read-Write)
SCPI.CALCulate(Ch).SELected.EQUation.TEXT = Data
Data = SCPI.CALCulate(Ch).SELected.EQUation.TEXT
This command sets/gets the equation in the Equation Editor for selected channel (Ch). For valid parameters that can be used in this equation, refer to the Equation Editor.
|
Parameter |
Data |
|
Description |
Sets/Gets the equation in the Equation Editor |
|
Data type |
Character string type (String) |
Dim strEq As String
SCPI.CALCulate(1).SELected.EQUation.STATE = True
EqState = SCPI.CALCulate(1).SELected.EQUation.State
SCPI.CALCulate(1).SELected.EQUation.TEXT = "Example=S21/(1-S11)"
strEq = SCPI.CALCulate(1).SELected.EQUation.TEXT
SCPI.CALCulate(Ch).SELected.EQUation.STATE
SCPI.CALCulate(Ch).SELected.EQUation.VALid
No equivalent key is available on the front panel for Equation Text but Equation Editor can be accessed through Display > Equation Editor.
:CALCulate{[1]-4}[:SELected]:EQUation:TEXT <string1>
:CALCulate{[1]-4}[:SELected]:EQUation:TEXT?
<string 1><newline><^END>
10 OUTPUT 717;":CALC1:EQU:TEXT?"
30 ENTER 717;A$