SCPI.CALCulate(Ch).EPARameters.SIMulate.IMMediate

Object Type

Method (Write Only)

Syntax

SCPI.CALCulate(Ch).EPARameters.SIMulate.IMMediate

Description

This command writes the simulation results into the memory trace, then set "Data & Mem" for the display setting. All traces related with impedance measurement are updated, even if CALCulate [1-4]: EPARameters: SIMulate: AUTO is set at OFF.

Examples

SCPI.CALCulate(1).EPARameters.SIMulate.IMMediate

Related Objects

SCPI.CALCulate(Ch).EPARameters.SIMulate.AUTO

Equivalent Key

There is no equivalent key is available on the front panel. However, the similar key is:

Analysis > Equivalent Circuit > Simulate > ON|OFF

 

When this softkey is turned ON, its equivalent to:

SCPI.CALCulate[1-4].EPARameters.SIMulate.AUTO ON + SCPI.CALCulate(Ch).EPARameters.SIMulate.IMMediate

 

When this softkey is turned OFF, its equivalent to:

SCPI.CALCulate[1-4].EPARameters.SIMulate.AUTO OFF

Equivalent SCPI Command

Syntax

:CALCulate{[1]-4}:EPARameters:SIMulate[:IMMediate]

Example of use

10 OUTPUT 717;":CALC1:EPAR:SIM"