Property (Read-Write)
SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.CENTer = Value
Value = SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.CENTer
This command sets/gets the center value used for the transformation function of the fault location display, for the active trace of the selected channel (Ch).
|
Parameter |
Value |
|
Description |
Center value |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
Varies depending on the frequency span and the number of points. |
|
Preset Value |
0 |
|
Unit |
ft (feet) or m (meters) |
|
Note |
If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set. |
Dim Cent as Double
SCPI.CALCulate(4).SELected.TRANsform.DISTance.CENTer = 1E-8
Cent = SCPI.CALCulate(4).SELected.TRANsform.DISTance.CENTer
SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.SPAN
SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.STARt
SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.STOP
SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.UNIT
Analysis > Fault Location > Center
:CALCulate{[1]-4}[:SELected]:TRANsform:DISTance:CENTer <numeric>
:CALCulate{[1]-4}[:SELected]:TRANsform:DISTance:CENTer?
{numeric} <newline><^END>
10 OUTPUT 717;":CALC1:TRAN:DIST:CENT 0"
20 OUTPUT 717;":CALC1:TRAN:DIST:CENT?"
30 ENTER 717;A