SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.LPFRequency

Object Type

Method (Write Only)

Syntax

SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.LPFRequency

Description

This command changes the frequency range to match with the low-pass type transformation of the transformation function of the fault location display, for the active trace of the selected channel ( Ch).

Examples

SCPI.CALCulate(4).SELected.TRANsform.DISTance.LPFRequency

Related Objects

SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.STATe

SCPI.CALCulate(Ch).SELected.TRANsform.DISTance.TYPE

Equivalent Key

Analysis > Fault Location > Set Freq Low Pass

Equivalent SCPI Command

Syntax

:CALCulate{[1]-4}[:SELected]:TRANsform:DISTance:LPFRequency

Example of use

10 OUTPUT 717;":CALC1:TRAN:DIST:LPFR"