Method (Write Only)
SCPI.CALCulate(Ch).SRL.CONNector(Pt).IMMediate
This command measures the terminated cable connected to the specified port ( Pt) and automatically sets the connector length and capacitance values for connector mismatch compensation, for the active trace of the selected channel ( Ch).
SCPI.CALCulate(2).SRL.CONNector(1).IMMediate
SCPI.CALCulate(Ch).SRL.CONNector(Pt).CAPacitance
SCPI.CALCulate(Ch).SRL.CONNector(Pt).LENGth
Analysis > SRL > Port1 Connector|Port2 Connector > Measure Connector
:CALCulate{[1]-4}:SRL:CONNector{[1]|2}:IMMediate
10 OUTPUT 717;":CALC1:SRL:CONN2:IMM"