Property (Read-Write)
SCPI.CALCulate(Ch).PARameter(Tr).DEFine = Param
Param = SCPI.CALCulate(Ch).PARameter(Tr).DEFine
This command sets/gets the measurement parameter of the selected trace (Tr), for the selected channel (Ch).
|
Parameter |
Param |
|
Description |
Measurement parameter |
|
Data Type |
Character string type (String) |
|
Range |
Select either one of the following:
|
|
Preset Value |
"S11" |
Dim MeasPara As String
SCPI.CALCulate(1).PARameter(1).DEFine = "s21"
MeasPara = SCPI.CALCulate(1).PARameter(1).DEFine
SCPI.CALCulate(Ch).SELected.ZPARameter.DEFine
SCPI.CALCulate(Ch).SELected.FORMat
Meas > S<XY> {X=1-2;Y=1-2}
Meas > Absolute > R1|R2|A|B
Meas > Gain-Phase > T/R|R|T
Meas > Impedance Analysis Menu
:CALCulate{[1]-4}:PARameter{[1]-4}:DEFine {S11|S21|S12|S22|A|B|R1|R2|TR|T|R}
:CALCulate{[1]-4}:PARameter{[1]-4}:DEFine?
{S11|S21|S12|S22|A|B|R1|R2|TR|T|R}<newline><^END>
10 OUTPUT 717;":CALC1:PAR1:DEF S21"
20 OUTPUT 717;":CALC1:PAR1:DEF?"
30 ENTER 717;A$