Property (Read-Write)
SCPI.CALCulate(Ch).SELected.LIMit.OFFSet.AMPLitude = Value
Value = SCPI.CALCulate(Ch).SELected.LIMit.OFFSet.AMPLitude
This command sets/gets the limit line offset of response for the active trace of selected channel (Ch). The setting of the limit line does not change even if the offset value is changed.
| 
 Parameter  | 
 Value  | 
| 
 Description  | 
 The limit line offset of Response (Vertical offset)  | 
| 
 Data type  | 
 Double precision floating point type (Double)  | 
| 
 Range  | 
 -5E8 to 5E8  | 
| 
 Preset value  | 
 0  | 
| 
 Unit  | 
 Varies depending on the data format. 
  | 
Dim LimOffset As Double
SCPI.CALCulate(1).SELected.LIMit.OFFSet.AMPLitude = -10
LimOffset = SCPI.CALCulate(1).SELected.LIMit.OFFSet.AMPLitude
SCPI.CALCulate(Ch).SELected.LIMit.STATe
SCPI.CALCulate(Ch).SELected.LIMit.OFFSet.MARKer
SCPI.CALCulate(Ch).SELected.LIMit.OFFSet.STIMulus
Analysis > Limit Test > Limit Line Offsets > Amplitude Offset
:CALCulate{[1]-4}[:SELected]:LIMit:OFFSet:AMPLitude <numeric>
:CALCulate{[1]-4}[:SELected]:LIMit:OFFSet:AMPLitude?
{numeric}<newline><^END>
10 OUTPUT 717;":CALC1:LIM:OFFS:AMPL -10"
20 OUTPUT 717;":CALC1:LIM:OFFS:AMPL?"
30 ENTER 717;A