Method (Write-only)
SCPI.DISPlay.UPDate.IMMediate
This command executes the display update once when the display update of the LCD screen is set to OFF (specifying False with the SCPI.DISPlay.ENABle object).
SCPI.DISPlay.ENABle = False
SCPI.DISPlay.UPDate.IMMediate
No equivalent key is available on the front panel.
:DISPlay:UPDate[:IMMediate]
10 OUTPUT 717;":DISP:UPD"