Parameter |
Cpt_m, Cpt_n |
Description |
Port number |
Data type |
Long integer type (Long) |
Range |
1 to 2 |
Note |
If the specified variable is out of the allowable setup range, an error occurs when executed. |
Since the variables (Cpt_m and Cpt_n) have no preset value, you cannot omit them. If you omit the variables (Cpt_m and Cpt_n) or if you specify the same port number to 2 port numbers, an error occurs when executed. Notice that when you specify 2 ports with the variables (Cpt_m and Cpt_n), the order of the 2 port numbers is arbitrary.