Parameter

Dnum

Description

The number of display mode
1: normal display
2: inverted display

Data type

Long integer type (Long)

Range

1 to 2

Preset value

1

Note

If the specified variable is out of the allowable setup range, an error occurs when executed.