No equivalent COM Commands
:MMEMory:LOAD:PROGram <string>
This command loads (or imports) a VBA project (a file with the .vba extension), a module (a file with the .bas extension), a user form (a file with the .frm extension) or a class module (a file with the .cls extension). If the specified file does not exist, an error occurs and the command is ignored.
|
Parameter |
String |
|
Description |
File name in which you want to load the VBA project |
|
Range |
254 characters or less |
|
Preset value |
"" |
10 OUTPUT 717;":MMEM:LOAD:PROG ""Test1/Test1_01.vba"""
10 OUTPUT 717;":MMEM:LOAD:PROG ""A:Test1_01.vba"""
Macro Setup > Load VBA Project