Method (Write Only)
SCPI.MMEMory.STORe.EPARameters = Value
This command saves the equivalent circuit parameters of an active channel into a CSV file at defined location.
|
Parameter |
Value |
|
Description |
Filename and destination |
|
Data Type |
Character string type (String) |
|
Range |
254 chars |
|
Preset Value |
- |
|
Unit |
- |
|
Resolution |
- |
Dim Var as String
Var = "C:\sample.csv"
SCPI.MMEMory.STORe.EPARameters = Var
There is no equivalent key available on the front panel. However, similar key which exports to TXT file is shown below:
Analysis > Equivalent Circuit > Export to TXT File...
:MMEMory:STORe:EPARameters
10 OUTPUT 717;":MMEM:STOR:EPAR Sample_Text"